How to decrease measurement time for the LTC DC2259->LTC DC2259?

Hi all,  I am doing research for system ID for battery systems and I need to measuring a single cell voltage and set the  discharge state of the balancing resistor at rate of less than 1 ms. My current set up is a laptop connected through a serial port to a LTC DC2026 Demo board connected to a LTC DC2259 battery stack monitor. Right now I am capable of doing this in about 2.4 ms and I believe that the majority of this time is used up in communication of data between the two demo boards and the serial communication to a laptop. Is there a way to speed up this process. Again I am only interested in a single cell.  Thanks for the help.

attachments.zip
Parents Reply Children
No Data