Post Go back to editing

ADP1047  THD&PF

im looking for a pfc for a new application

input voltage: 380Vac to 440Vac 50Hz.

output voltage: 700V. 750V is possible too.

output power 2KW.

switching freq: 200Khz.

we dont want to use interleave solution.

 

the main demand is PF>0.99 and THD<3%.

can the ADP1047 meed those damands?

 

can you provide the eval board or similar app THD and PF spread sheet results from 20%Load to 100%Load?

 

Thanks,

Dudu Dayan

Parents
  • hi again,

    1. are you sure about the results?

       the THD should increase with input voltage. So the THD at 180Vac is 2.9% and at 220Vac is 2.5% why is that?

    2. Moreover, in your opinion, how does the PFC inductor infuence THD? i think that higher inductance is good for THD due to CCM operation at all AC line shape.

Reply
  • hi again,

    1. are you sure about the results?

       the THD should increase with input voltage. So the THD at 180Vac is 2.9% and at 220Vac is 2.5% why is that?

    2. Moreover, in your opinion, how does the PFC inductor infuence THD? i think that higher inductance is good for THD due to CCM operation at all AC line shape.

Children
No Data