Post Go back to editing

ADP1047  THD&PF

im looking for a pfc for a new application

input voltage: 380Vac to 440Vac 50Hz.

output voltage: 700V. 750V is possible too.

output power 2KW.

switching freq: 200Khz.

we dont want to use interleave solution.

 

the main demand is PF>0.99 and THD<3%.

can the ADP1047 meed those damands?

 

can you provide the eval board or similar app THD and PF spread sheet results from 20%Load to 100%Load?

 

Thanks,

Dudu Dayan

Parents
  • Hi Dudu Dayan,

    The ADP1047 (single phase) can support all the features in your query. However, about THD - that is something that depends on the inductor and mainly the external EMI filter. This part is controller independent.

    We've done power stages that were at 3.3kW which a pf> 0.99. The current THD is very much dependent on the control loop and that in turn is dependent on the inductor used.

    Lt Comm Data

Reply
  • Hi Dudu Dayan,

    The ADP1047 (single phase) can support all the features in your query. However, about THD - that is something that depends on the inductor and mainly the external EMI filter. This part is controller independent.

    We've done power stages that were at 3.3kW which a pf> 0.99. The current THD is very much dependent on the control loop and that in turn is dependent on the inductor used.

    Lt Comm Data

Children
No Data