Is there an LTSpice model for LT4295?

I wanted to do LTSpice simulations on a POE design and can't find a model for LT4925. Is one going to be available soon?

Parents
  • 0
    •  Analog Employees 
    on Jun 16, 2018 4:48 AM

    Hello,

    There currently is not a released LT4295 LTSpice model. I've listed several options below.

    Are you trying to simulate the IEEE 802.3bt PD interface? If so, there's a LTSpice model for LT4294 which models the interface.

    Are you trying to simulate the DC/DC converter? If so, the LT4276 is very similar and can be used to model the converter inside the LT4295.

    Best Regards,

    Eric

Reply
  • 0
    •  Analog Employees 
    on Jun 16, 2018 4:48 AM

    Hello,

    There currently is not a released LT4295 LTSpice model. I've listed several options below.

    Are you trying to simulate the IEEE 802.3bt PD interface? If so, there's a LTSpice model for LT4294 which models the interface.

    Are you trying to simulate the DC/DC converter? If so, the LT4276 is very similar and can be used to model the converter inside the LT4295.

    Best Regards,

    Eric

Children
No Data