It's good by a reference value, not the guarantee, so please tell me below.
How many is time looseness until the level of FAULT is switched over after SHDN is released?
Hello,
The FAULT signal is actually valid regardless of the state of the SHDN pin. SHDN is only relevant to whether the charger is enabled or not.
Regards,
Zack
Thank you for your answer.
We need a little more clarity in this question. What spec are you looking for?
Do you mean the max amount of time for the FAULT reading to be valid after SHDN goes low? Or SHDN goes high? Is there a spec that you are referencing that you would like a min/max value for?
>Do you mean the max amount of time for the FAULT reading to be valid after SHDN goes low? Or SHDN goes high? >Is there a spec that you are referencing that you would like a min/max value for?
Yes,I want to min/max value for ”the max amount of time for the FAULT reading to be valid after SHDN goes low”