Post Go back to editing

LT8602 and FPGA

I'd like to use LT8602 to power FPGA like XILINX SPARTAN7 because it is possible to generate 4 different voltages in sequence and because in my board the input voltage is 24V.

The 4 currents requested from my FPGA are under 1A and so I think that the LT8602 could be a good solution because it occupies a very small space in  the board.

I'm worried about the transient response of the LT8602 because in the datasheet I did not find any information.

Can anybody answer me?

Thank you, Nicola