KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD5235
Production
The AD5235 is a dual-channel, nonvolatile memory, digitally
controlled potentiometer with 1024-step resolution, offering
guaranteed maximum low resistor...
Datasheet
AD5235 on Analog.com
Hello,
I want to generate a variable bias current for an IC from 5uA to 20uA. I am doing this with a TI current source and AD SPI programmable variable resistor, the datasheet set up and my schematic are attached in the pictures. Looks simple enough, I change the programmable resistance values through SPI and this changes the Bias Current.
I supply 5V power to the PCB which is used to power most of the ICs on the board.
Problem:
When I connect the Vsupply (which is 3.3V generated by a TI LDO: http://www.ti.com/lit/ds/symlink/tps7a8300.pdf) to the current source by means of a jumper then there seems to be a short circuit.
I assume that somewhere in my schematic I connected the ICs incorrectly because when I measure the resistance between the 5V line and GND I get 500Ohms. When I removed these components from the PCB the shorting problem went away.
Thank you!
ambugua - Moved from StudentZone (Analog Dialogue) to Power Management. Post date updated from Monday, October 16, 2017 10:07 PM UTC to Tuesday, June 24, 2025 11:46 PM UTC to reflect the move.
So may be the pot is set so that W and B are shorted? Mey be try configuring it while its disconnected and then put on the jumper.