Post Go back to editing

Using LT3798 sample circuit for 5 V 3 A output

Thread Summary

The user seeks to modify an LT3798/LT8309 5V, 2A isolated converter to output 5V, 3A using a Wurth Electronics transformer. The support engineer suggests using the 750811101 transformer and making specific changes to the circuit, including doubling C3, changing R6 to 4.32K, and doubling or tripling the output capacitance. For the 750811611 transformer, R6 should be increased to about 7K, and secondary windings should be connected in parallel. Testing is required to ensure the converter meets the 5V, 3A requirement.
AI Generated Content
I am interested in using the given example circuit (linked below) for my senior design project and was wondering what transformer (part # off the shelf) I could use to provide 5 V 3 A output? (Preferably from Wurth Electronic) Additionally, I am interesting in using this for a 5 V 3 A output, what changes might I need to make to the circuit in order to get 3 A output instead of 2.2? Thank you very much for your time.

Thread Notes

Parents
  • I managed to get 5v and 1.6 A using the circuit shown as 403-5v. I'm unable to get it to 3 A as far as I can tell, is this approach feasible? Additionally, I attempted to make the suggested changes to the circuit and it's completely stopped working (shown as 403-2). Do you have a full schematic I might be able to see for the full wiring layout? 

    403-5v:

    403-2:

    Thanks!!

Reply
  • I managed to get 5v and 1.6 A using the circuit shown as 403-5v. I'm unable to get it to 3 A as far as I can tell, is this approach feasible? Additionally, I attempted to make the suggested changes to the circuit and it's completely stopped working (shown as 403-2). Do you have a full schematic I might be able to see for the full wiring layout? 

    403-5v:

    403-2:

    Thanks!!

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.