KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
LT3798
Production
The LT3798 is a constant-voltage/constant-current isolated flyback controller that combines active power factor correction (PFC) with no opto-coupler required...
Datasheet
LT3798 on Analog.com
GenevaCooper - Moved from StudentZone (Analog Dialogue) to Power Management. Post date updated from Friday, March 30, 2018 12:18 AM UTC to Wednesday, June 25, 2025 1:41 AM UTC to reflect the move.
I would suggest you try the 750811611 option, with secondary windings in parallel. The leakage inductance is on the high side, but the other option is not much better.
Follow the list I gave before, except increase R6 to about 7K, instead of 4.32K. (might have to readjust this resistor later).
To make life easier, I would not start with the circuits in the dashed boxes, for now. You can add these options later, after you get the converter working.
To implement this suggestion, connect IC bias and output rectification as shown below. You can choose a diode option from the datasheet. Diode might need a heat-sink, once you get 3A of output current.
Best of luck!
I would suggest you try the 750811611 option, with secondary windings in parallel. The leakage inductance is on the high side, but the other option is not much better.
Follow the list I gave before, except increase R6 to about 7K, instead of 4.32K. (might have to readjust this resistor later).
To make life easier, I would not start with the circuits in the dashed boxes, for now. You can add these options later, after you get the converter working.
To implement this suggestion, connect IC bias and output rectification as shown below. You can choose a diode option from the datasheet. Diode might need a heat-sink, once you get 3A of output current.
Best of luck!