Post Go back to editing

Using LT3798 sample circuit for 5 V 3 A output

Thread Summary

The user seeks to modify an LT3798/LT8309 5V, 2A isolated converter to output 5V, 3A using a Wurth Electronics transformer. The support engineer suggests using the 750811101 transformer and making specific changes to the circuit, including doubling C3, changing R6 to 4.32K, and doubling or tripling the output capacitance. For the 750811611 transformer, R6 should be increased to about 7K, and secondary windings should be connected in parallel. Testing is required to ensure the converter meets the 5V, 3A requirement.
AI Generated Content
I am interested in using the given example circuit (linked below) for my senior design project and was wondering what transformer (part # off the shelf) I could use to provide 5 V 3 A output? (Preferably from Wurth Electronic) Additionally, I am interesting in using this for a 5 V 3 A output, what changes might I need to make to the circuit in order to get 3 A output instead of 2.2? Thank you very much for your time.

Thread Notes

Parents
  • I can't find any Ltspice files for Wurth 750811101 but I do have them for 750811618 and 750811611 which I was told by Wurth should also work for this application. I've been playing with the circuit values but can't seem to get 5 V 3 A from either of these transformers. What changes would you suggest in the case that I was using one of those two?

    Thank you so much for replying with such helpful information! 

Reply
  • I can't find any Ltspice files for Wurth 750811101 but I do have them for 750811618 and 750811611 which I was told by Wurth should also work for this application. I've been playing with the circuit values but can't seem to get 5 V 3 A from either of these transformers. What changes would you suggest in the case that I was using one of those two?

    Thank you so much for replying with such helpful information! 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.