Post Go back to editing

Using LT3798 sample circuit for 5 V 3 A output

Thread Summary

The user seeks to modify an LT3798/LT8309 5V, 2A isolated converter to output 5V, 3A using a Wurth Electronics transformer. The support engineer suggests using the 750811101 transformer and making specific changes to the circuit, including doubling C3, changing R6 to 4.32K, and doubling or tripling the output capacitance. For the 750811611 transformer, R6 should be increased to about 7K, and secondary windings should be connected in parallel. Testing is required to ensure the converter meets the 5V, 3A requirement.
AI Generated Content
I am interested in using the given example circuit (linked below) for my senior design project and was wondering what transformer (part # off the shelf) I could use to provide 5 V 3 A output? (Preferably from Wurth Electronic) Additionally, I am interesting in using this for a 5 V 3 A output, what changes might I need to make to the circuit in order to get 3 A output instead of 2.2? Thank you very much for your time.

Thread Notes

Parents
  • This converter was done for a specific application, with emphasis on efficiency and minimum power consumption at no load.

    There is a transformer from Wurth Electronics, 750811101, which can do 5V at 3A, but needs to be tested with the configuration called out.

    The following are recommended changes to test the converter (please refer to the schematic for designators):

    1. Double the value of C3 (input cap).

    2. Change value of R6 to 4.32K (feedback resistor).

    3. Double or triple the total output capacitance value. Ensure capacitors have at least 4.5A of ripple current capability.

    Other minor value changes might be needed, but the above changes should bring you close to the goal.

    Again, testing is required to ensure converter meets your requirements.

Reply
  • This converter was done for a specific application, with emphasis on efficiency and minimum power consumption at no load.

    There is a transformer from Wurth Electronics, 750811101, which can do 5V at 3A, but needs to be tested with the configuration called out.

    The following are recommended changes to test the converter (please refer to the schematic for designators):

    1. Double the value of C3 (input cap).

    2. Change value of R6 to 4.32K (feedback resistor).

    3. Double or triple the total output capacitance value. Ensure capacitors have at least 4.5A of ripple current capability.

    Other minor value changes might be needed, but the above changes should bring you close to the goal.

    Again, testing is required to ensure converter meets your requirements.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.