I plan on using the LTC7862 surge stopper circuit in one of my designs. The load current maximum requirement is 25 Amps at 28 VDC. So nominal voltage is 28 VDC and then there is a surge pulse of 100V at 50 msec. This surge voltage occurs 5 times with 5 seconds in between each. I have a few questtions:
- For the top side MOSFETs I have x2 IPT015N10N5. Each is 169nC typ and max 211nC. So, the total gate charge driving would be 338nC typ and 422nC max. Can the LTC7862 drive both these MOSFET gates properly with that gate charge from pin TG?
- For the bottom side MOSFETs I have x2 IPT015N10N5 MOSFETS as well. Can the LTC7862 drive these okay as well from BG? Do I need one MOSFET only or two based on my load current?
- How to determine the Gate drive loss inside the LTC7862? Is it acceptable range for these MOSFETs? Is the chip within thermal limits to drive these FETS?
- Is there a max gate capacitance the TG and BG pins can drive, or can they drive any power MOSFETS and the larger the gate capacitance the slower the turn on time?
- If the IPT015N10N5 isn’t okay to use than what Power MOSFET would you recommend?
- Are there gate resistor requirements to meet or is 4.7 ohms okay?
- Any other design considerations I need to pay attention to as well or everything looks okay from a schematic view?