Post Go back to editing

MAX77972 BC1.2 Not always completing

Category: Hardware
Product Number: MAX77972

I'm using the MAX77972 chip for USB 2.0 only charging.  The CC pins are not available to me, so CC pin detection is disabled.  The DATAMUX bit is set, so upon completion of BC1.2 detection, D+ and D- are routed to the CPU for data communication.  I have reproduced this issue on the MAX77972 EV KIT board, with J5 1-2 jumpered.

Most of the time, BC1.2 completes and returns CDP 1.5A as shown below.
(Traces are DATAMUX, CHGIN, DPCHG, CNCHG)

Sometimes the DATAMUX low transition happens shorter, sometimes later.

But maybe 1 in 20 times, DATAMUX goes low before BC1.2 can complete, and it defaults back to SDP 500 mA.

Any idea what could be causing this, on both my PCB and the EVKIT?  If the DATAMUX bit is set to 0, DATAMUX stays high and BC1.2 always works properly.  Changing the data contact detection timeout from 0.9s to 2s seems to do nothing.

I'm considering putting my own external 1 second delay from CHGIN to switch the USB mux, and ignoring the supplied DATAMUX bit.  Has anyone done that on other designs (MAX77972 or not) and should it reliable?  The DATAMUX output seems to be unreliable.

Thanks for any help!

  • Thanks for sending captures and for reproducing this on the EV kit. 

    I’m looking into DATAMUX behavior and your question on using external delay.

    One thing I wanted to clarify: 

    Does your software change any MAX77972 settings during tests? Or do you just let it run after the initial setup?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.