Post Go back to editing

How do I set straps on the EVAL-LT7930 to just run top supply

Category: Hardware
Product Number: LT7930

URGENT:    Please help FAST

Datasheet seems clear but I seek confirmation on this point so I ask now that we have eval board

To run just top supply on EVAL-LT7930-AZ board I know I would have to change these things:   Tell me if there is more

1)  On both top and bottom of supply 2  cut the fat traces to output under R63 (top) and R191 (bottom)

2) per the 'PHASE CONNECT' part of EVAL board schematic:

A) Remove R1 to not make CLKOUT_1 go to SYNC_2  thus bottom supply will have it's SYNC_2 disconnected and run independantly

B) Remove R4 Isolates  ITH_1 and ITH_2

C) Remove R5   Isolates VFB_1 and VFB_2

IS THERE SOME STRAP FOR PHASMD that is required to run independant?   Datasheet shows PHASMD grounded for standalone unit

SECONDLY:    ON the EVAL board is SGND and PGND both connected to PGND?

(Also ensure R2 and R3 are out to avoid connect of both RUN and SS lines

Will this allow separate supplies that can be changed for our desired voltages on its own?

Thank you,  Mark Johnston

Parents
  • Thank you for the reply.

    I have managed to get the two halfs running independently. I do not need any other doc or assist to explain  how to make it happen. I'm not going to restate how I did it but it is mostly in earlier thread here.   My email is purely feedback for consideration for future customers to have a more pleasant experience.

    Even if the board remains as it is now your team and customers would benefit from simple layout changes with very short top traces to parts a customer may wish to reconfigure to be able to be removed and reconfigured with flux and a 'normal' top side common heat wand. 

    There are a great many test points and the ability to reconfigure and I salute your team for the well thought out 'schematic'.      I have done massive 0402 tiny rework in years past and can say this board is the very hardest to do part lifting and swapping of any board I have seen due to extreme heat sinking on basically all parts. that seem designed to be swapped.   Full backside IR heating and extreme hot air wand temps are required and should not be required for parts that do not have some need to be greatly heat sinked like 0 ohm jumpers.

    As a minimum the resistor to set voltage level and perhaps  the one to set switching frequency as much easier to change by a customer.  Voltage for sure and switching freq perhaps not as important as that impacts other parts of the design.  

    Treat my comment simply as feedback to allow the wonderful re-config 0 ohm jumpers and parts like voltage change to  LT7930. It is a wonderful thing to have the board show multiple LT7930s.  I worked out how to separate the 2 supplies and am not requesting help to ask your team to explain that change.

    Thanks again for the fast reply,   Mark

Reply
  • Thank you for the reply.

    I have managed to get the two halfs running independently. I do not need any other doc or assist to explain  how to make it happen. I'm not going to restate how I did it but it is mostly in earlier thread here.   My email is purely feedback for consideration for future customers to have a more pleasant experience.

    Even if the board remains as it is now your team and customers would benefit from simple layout changes with very short top traces to parts a customer may wish to reconfigure to be able to be removed and reconfigured with flux and a 'normal' top side common heat wand. 

    There are a great many test points and the ability to reconfigure and I salute your team for the well thought out 'schematic'.      I have done massive 0402 tiny rework in years past and can say this board is the very hardest to do part lifting and swapping of any board I have seen due to extreme heat sinking on basically all parts. that seem designed to be swapped.   Full backside IR heating and extreme hot air wand temps are required and should not be required for parts that do not have some need to be greatly heat sinked like 0 ohm jumpers.

    As a minimum the resistor to set voltage level and perhaps  the one to set switching frequency as much easier to change by a customer.  Voltage for sure and switching freq perhaps not as important as that impacts other parts of the design.  

    Treat my comment simply as feedback to allow the wonderful re-config 0 ohm jumpers and parts like voltage change to  LT7930. It is a wonderful thing to have the board show multiple LT7930s.  I worked out how to separate the 2 supplies and am not requesting help to ask your team to explain that change.

    Thanks again for the fast reply,   Mark

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.