Post Go back to editing

Timing behavior of the PGOOD pin and INTVCC output

Thread Summary

The user is concerned about potential startup glitches on the PGOOD pin when tied to the 3.3V INTVCC output. The final answer confirms that while the datasheet does not specify the timing relationship between INTVCC ramp-up and PGOOD pull-down activation, the intended behavior is for PGOOD to remain low until VOUT is within ±8% of regulation. To mitigate any risk of downstream device activation due to a brief glitch, the engineer suggests adding an RC filter or using a buffer/comparator with a defined threshold.
AI Generated Content
Category: Hardware
Product Number: LTM4622

The datasheet recommends tying PGOOD to the 3.3V output of the internal LDO (INTVCC pin). I want to verify that if I do this, the PGOOD pin will be pulled to ground internally before the output of INTVCC can pull up this open-drain pin to 3.3V via the external pullup resistor. If PGOOD starts to rise before it gets pulled to ground, I would like to know how high the voltage can possibly get - I do not want any startup glitch high enough to turn the other downstream device on. I did a simulation with the LTSpice model but did not see any rise on PGOOD which surprised me since I would think that INTVCC would output 3.3V before the pins gets pulled to ground - mainly because the circuitry that pulls the open-drain FET to ground is most likely power by that internal 3.3V LDO. So I am not sure if I can trust the simulation model or not. 

Parents
    • PGOOD1/PGOOD2 are open‑drain outputs monitoring a ±8% window around VOUT, with a pull‑down resistance of about 20 Ω at 1 mA when they are asserted low.

    • INTVCC is the internal 3.3 V regulator that powers the internal control circuitry; typical 3.3 V, abs max 3.6 V.

    • The datasheet explicitly allows PGOOD to be pulled up to INTVCC (PGOOD abs max –0.3 V to 18 V, INTVCC –0.3 V to 3.6 V).

     

    What is not specified anywhere is a quantitative timing relationship between:

    • INTVCC ramp‑up
      Internal logic/PGOOD circuitry becoming active

    • Assertion of the PGOOD pull‑down during startup

     

    So from available documentation we cannot state a guaranteed maximum “startup glitch” voltage on PGOOD when its pull‑up is tied to INTVCC.

    However, two points are clear:

    • Intended behavior: PGOOD is held low (or at least not released high) until VOUT is within ±8% of regulation; there is also a ~40 µs blanking delay on PGOOD falling to avoid glitches during transients. This is consistent with your LTspice result showing no visible rise on PGOOD when pulled up to INTVCC.

    • Strength of pull‑down: Once the PGOOD pull‑down is active, its resistance is ≈20 Ω at 1 mA. With a typical pull‑up of 10 kΩ to INTVCC, the node is strongly clamped near ground as soon as the pull‑down turns on. Any vulnerable window would be only before that pull‑down is enabled, and that window is not specified.

    Because there is no formal spec for that internal timing, you should not rely on “no startup glitch” as a guaranteed behavior if a brief glitch could turn on a sensitive downstream device.

    To avoid any risk of downstream startup due to a small PGOOD glitch when pulled up to INTVCC, the usual mitigations are:

    • Add an RC on PGOOD (pull‑up resistor + small capacitor to GND) so that any very short high‑Z interval before the pull‑down engages cannot charge the node high enough to cross the downstream enable threshold.

    • Use a buffer/comparator with a defined threshold (e.g., ≥1.5–2 V) between PGOOD and the downstream enable, so minor analog excursions on PGOOD never reach the logic threshold.

    • Alternatively, pull PGOOD up to a system rail that only comes up after LTM4622 outputs are in regulation.
       

    Your LTspice observation (no rise on PGOOD) is consistent with the intended behavior, but since the model is not a formal timing spec, I would treat it as qualitative confirmation and still implement one of the above safeguards if an unintended downstream turn‑on would be problematic.

    If you share the downstream device’s enable threshold and your chosen PGOOD pull‑up resistor value, I can suggest concrete R/C values or a buffer threshold that will give you comfortable margin.

     

     

     

     

     

     

     

     

Reply
    • PGOOD1/PGOOD2 are open‑drain outputs monitoring a ±8% window around VOUT, with a pull‑down resistance of about 20 Ω at 1 mA when they are asserted low.

    • INTVCC is the internal 3.3 V regulator that powers the internal control circuitry; typical 3.3 V, abs max 3.6 V.

    • The datasheet explicitly allows PGOOD to be pulled up to INTVCC (PGOOD abs max –0.3 V to 18 V, INTVCC –0.3 V to 3.6 V).

     

    What is not specified anywhere is a quantitative timing relationship between:

    • INTVCC ramp‑up
      Internal logic/PGOOD circuitry becoming active

    • Assertion of the PGOOD pull‑down during startup

     

    So from available documentation we cannot state a guaranteed maximum “startup glitch” voltage on PGOOD when its pull‑up is tied to INTVCC.

    However, two points are clear:

    • Intended behavior: PGOOD is held low (or at least not released high) until VOUT is within ±8% of regulation; there is also a ~40 µs blanking delay on PGOOD falling to avoid glitches during transients. This is consistent with your LTspice result showing no visible rise on PGOOD when pulled up to INTVCC.

    • Strength of pull‑down: Once the PGOOD pull‑down is active, its resistance is ≈20 Ω at 1 mA. With a typical pull‑up of 10 kΩ to INTVCC, the node is strongly clamped near ground as soon as the pull‑down turns on. Any vulnerable window would be only before that pull‑down is enabled, and that window is not specified.

    Because there is no formal spec for that internal timing, you should not rely on “no startup glitch” as a guaranteed behavior if a brief glitch could turn on a sensitive downstream device.

    To avoid any risk of downstream startup due to a small PGOOD glitch when pulled up to INTVCC, the usual mitigations are:

    • Add an RC on PGOOD (pull‑up resistor + small capacitor to GND) so that any very short high‑Z interval before the pull‑down engages cannot charge the node high enough to cross the downstream enable threshold.

    • Use a buffer/comparator with a defined threshold (e.g., ≥1.5–2 V) between PGOOD and the downstream enable, so minor analog excursions on PGOOD never reach the logic threshold.

    • Alternatively, pull PGOOD up to a system rail that only comes up after LTM4622 outputs are in regulation.
       

    Your LTspice observation (no rise on PGOOD) is consistent with the intended behavior, but since the model is not a formal timing spec, I would treat it as qualitative confirmation and still implement one of the above safeguards if an unintended downstream turn‑on would be problematic.

    If you share the downstream device’s enable threshold and your chosen PGOOD pull‑up resistor value, I can suggest concrete R/C values or a buffer threshold that will give you comfortable margin.

     

     

     

     

     

     

     

     

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.