Post Go back to editing

LTC3766 Synchronization

Category: Datasheet/Specs
Product Number: LTC3766

Hi all,

I'm designing an isolated forward active clamp converter with LTC3765/LTC3766 ICs. The LTC3766 has FS/SYNC input to produce switching clock. Its datasheet claims this pin is synchronized on falling edge crossing 2V. I've connected LTC1799 output to this FS/SYNC input, while clock is set to 470KHz. I'm trying simulating this circuit. After RUN pin crosses 1.22V, and LTC3766 starts producing switching pulses, it operates at high switching frequency of ~720KHz instead of locking on an external 470KHz/5V squarewave clock, and after couple of clocks an output shuts down. I've seen some circuit at figure 6 of LTC3766 datasheet showing clock connectivity for a case where input clock is postponed relatively to IC enable. In my case 470KHz clock starts much earlier. Can somebody explain this phenomena?

Sincerely,

Alex

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.