Post Go back to editing

5V in to 3.3V out power up at ~2.8V

Category: Hardware
Product Number: LT1765

Hello,

We have an old design with LT1765EFE that we recently produced 25 new units.

The LT1765EFE is powering a uC and peripheral that consume total of 200mA.

During testing of the boards we saw that 10 of 25 boards output ~2.8V instead of 3.3V after power-up.

During invetigation, we saw that when turning on the lab power supply 5V the voards fail at ~2.8V, but when connecting the wire of the 5V while the lab power supply was already at 5V the board power-up correctly to 3.3V.

When measuring with a scope we saw that the high power-up of the 5V input was making the difference..

Below is the circuit  of the LT1765EFE on the board.

We try to do the following debug steps but nothing solved the problem.

  1. Increase C1 to 220nF. 
  2. Remove C2.
  3. Measured R25, R26 and R27 and verified their values.
  4. Removed and placed new capacitors instead of C7 and C8 to make sure that it is not a mistake in assembly.
  5. Removed R27 and C7 and place 2.2nF capacitor instead of C8 as reccomended in the data sheet.
  6. Replace the inductor with a higher Isat inductor from coilcraft XAL6060.
  7. Replace the LT1765EFE.
  8. Perorm simulation with LTspice. Looks OK on simulation.
  9. Replace the Lab power supply with two other types.
  10. On a failed power-up, when the output is stuck at ~2.8V, VC pin is stuck at 1.9V. well above the 0.4V to 0.9V region in normal operation. the VC pin = ~0.45V after power-up after a good power-up.
    During simulation it shows that the VC pin increase to 1.5V but then decrease to ~0.45V at the end of power-up. maybe the problem is in the device shourt circuit protection.
  11. Tie SHDN pin to VIN.

Please advise what else we can do to fix the problem.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.