Post Go back to editing

LTC4286 comms when VDD not present

Thread Summary

The user inquires about externally powering the I2C communications of the LTC4286 to avoid timeouts when VDD is not present. The final answer confirms that the DVCC pin cannot be used for external power and that VDD is necessary for the status registers to function. No alternative solutions are provided.
AI Generated Content
Category: Hardware
Product Number: LTC4286

Hello,

We have been working with the LTC4286 as a soft start power switch for some time and it works great for that application. The one downside is that the internal I2C comms are powered from the DVDD which does not exist if VDD is not present. When software polls for status it then has to timeout delaying telemetry gathers.

Is there a means to externally power the communications portion of the chip so that our software can still poll the device for status? Perhaps a diode OR to the VDD pin from a 5V supply? Is there another approach perhaps?

Thanks,

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.