Post Go back to editing

LT3045 Loop-Gain Measurement: Where Should the Injection Resistor Be Placed?

Category: Hardware
Product Number: LT3045

I would like to measure the LT3045 control-loop response and generate a Bode plot using a frequency-response analyzer. What is the recommended way to break the loop for this measurement?

Should a small injection resistor be inserted in series between the output capacitor connection and the OUTS sense pin, with the analyzer connected across that resistor? If so, what resistance range works well without significantly disturbing normal operation?

Edit Notes

...make sure AI content is affirmed.
[edited by: ARad at 3:35 PM (GMT -4) on 2 Oct 2026]
Parents
    •  Analog Employees 
    on Oct 2, 2026 11:38 AM Contains AI Generated Content
    0

    Yes. A practical way to measure the LT3045 loop gain is to open the remote-sense path and install an injection resistor between the output-capacitor connection and the OUTS pin. Connect the frequency-response analyzer across this resistor in the analyzer’s normal loop-injection configuration.

    A 10 Ω resistor has worked well in the lab, and the exact value is not critical; approximately 10 Ω to 100 Ω should be suitable. The resistor provides a convenient AC injection point while maintaining the LT3045’s normal DC output-sense connection.

    Make the measurement with the regulator operating at the intended input voltage, output voltage, load current, and output-capacitor configuration, because these conditions can affect the measured loop response.

    I uploaded a schematic that shows the injection resistor and the frequency-response analyzer connection.  I also uploaded the results of the Bode plot.   

    dc3158a-schematic.pdf

    LT3041 DC3158A 5VIN 3.3VOUT at 500mA_0.pdf

Reply
    •  Analog Employees 
    on Oct 2, 2026 11:38 AM Contains AI Generated Content
    0

    Yes. A practical way to measure the LT3045 loop gain is to open the remote-sense path and install an injection resistor between the output-capacitor connection and the OUTS pin. Connect the frequency-response analyzer across this resistor in the analyzer’s normal loop-injection configuration.

    A 10 Ω resistor has worked well in the lab, and the exact value is not critical; approximately 10 Ω to 100 Ω should be suitable. The resistor provides a convenient AC injection point while maintaining the LT3045’s normal DC output-sense connection.

    Make the measurement with the regulator operating at the intended input voltage, output voltage, load current, and output-capacitor configuration, because these conditions can affect the measured loop response.

    I uploaded a schematic that shows the injection resistor and the frequency-response analyzer connection.  I also uploaded the results of the Bode plot.   

    dc3158a-schematic.pdf

    LT3041 DC3158A 5VIN 3.3VOUT at 500mA_0.pdf

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.