Post Go back to editing

How to implement the wake-up using a pushbutton switch and without connecting the USB on MAX17320?

Category: Hardware
Product Number: MAX17320

I would like to wakeup MAX17320 using a pushbutton switch.

The datasheet shows a circuit but it is not working on my setup:

What is the best way to do it?

Parents
  • Hi  ,

    Thanks, that rules out the NVM settings. PBen is set in both nConfig and Config, so pushbutton wake is configured correctly.

    To narrow down the cold-boot case, could you check:

    1. Right after a cold connect, before pressing the button, does the IC respond on I²C? If so, please read ProtStatus and HProtCfg2 (0x0F1). This tells us whether the part is asleep, or awake with the FETs held off.
    2. How are the cells connected during a cold boot? If they go on one at a time, the IC may see an undervoltage cell and enter Undervoltage Shutdown, which can only be exited by connecting a charger, not by the button. Does the issue still happen if both cells are connected at once?
    3. What powers the ALRT pull-up? Please scope ALRT through the cold connect and the button press. ALRT should idle high and stay low for more than ~100 ms when the button is pressed.
    4. Does connecting a charger wake the part on a cold boot?

    Best,
    Doug

Reply
  • Hi  ,

    Thanks, that rules out the NVM settings. PBen is set in both nConfig and Config, so pushbutton wake is configured correctly.

    To narrow down the cold-boot case, could you check:

    1. Right after a cold connect, before pressing the button, does the IC respond on I²C? If so, please read ProtStatus and HProtCfg2 (0x0F1). This tells us whether the part is asleep, or awake with the FETs held off.
    2. How are the cells connected during a cold boot? If they go on one at a time, the IC may see an undervoltage cell and enter Undervoltage Shutdown, which can only be exited by connecting a charger, not by the button. Does the issue still happen if both cells are connected at once?
    3. What powers the ALRT pull-up? Please scope ALRT through the cold connect and the button press. ALRT should idle high and stay low for more than ~100 ms when the button is pressed.
    4. Does connecting a charger wake the part on a cold boot?

    Best,
    Doug

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.