I would like to wakeup MAX17320 using a pushbutton switch.
The datasheet shows a circuit but it is not working on my setup:

What is the best way to do it?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
MAX17320
Recommended for New Designs
The MAX17320 is a 38µA IQ stand-alone pack-side fuel gauge IC with protector, battery internal self-discharge detection, and optional SHA-256 authentication...
Datasheet
MAX17320 on Analog.com
I would like to wakeup MAX17320 using a pushbutton switch.
The datasheet shows a circuit but it is not working on my setup:

What is the best way to do it?
RAM Config (00Bh) reads 0x2610.
nConfig = 0x2690
PBen = 1
nConfig = 0x2690
nPackCfg 0xA100
nProtCfg 0x0100 (DeepShip 0, ALRT override 0)
nODSCTh 0x0A04
nBalTh 0x046A
RAM Config (00Bh) reads 0x2610.
nConfig = 0x2690
PBen = 1
nConfig = 0x2690
nPackCfg 0xA100
nProtCfg 0x0100 (DeepShip 0, ALRT override 0)
nODSCTh 0x0A04
nBalTh 0x046A