Post Go back to editing

MAX17262 with LiPo batteries

Thread Summary

The MAX17262 supports Li-Po batteries, as it is compatible with Li+ and variants, including LiFePO4. The ModelID field allows for different lithium chemistry models, covering standard lithium-ion chemistries, which include Li-Po cells. For more details, refer to the Analog Devices FAQ on lithium polymer battery compatibility.
AI Generated Content
Category: Hardware
Product Number: MAX17262

For MAX17262, Does it suitable for Li-Po ( lithium-batteries) batteries as it's not mentioned in the datasheet

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.