For MAX17262, Does it suitable for Li-Po ( lithium-batteries) batteries as it's not mentioned in the datasheet
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX17262
Production
The MAX17262 is an ultra-low power fuel-gauge IC which implements the Maxim ModelGaugeâ„¢ m5 algorithm. The IC monitors a single-cell battery pack and...
Datasheet
MAX17262 on Analog.com
For MAX17262, Does it suitable for Li-Po ( lithium-batteries) batteries as it's not mentioned in the datasheet
The datasheet states that MAX17262 supports "Li+ and variants including LiFePO4" and provides different lithium chemistry models via the ModelID field. These models cover standard lithium‑ion chemistries, which include typical Li‑Po cells (Li‑Po is a form of Li‑ion with nearly identical electrical characteristics)
You can also refer to our FAQ: Are Maxim lithium ion battery chargers and fuel gauges compatible with lithium polymer batteries? - FAQs - Battery Management System Library - EngineerZone