Dear Sir, Madam,
I would like to use the LTM4644 to generate 4 supplies, 3.3V 2.5A, 1.8V 0.6A, 0.9V 0.5A and 1.15V 1A.
I simulate the design with LTPowerCad.
I see all the IL Riple of all ouput under the threshold 30%.
See the simulation file
28% for the 3.3V, 29% for the 1.8V, 18% for the 0.9V and 22% for the 1.15V.
I can not change the fsw frequency to improve the IL riple, the fsw it is fixed at 1MHz.
The only way to imrove it is to upper the VIN voltage.
It is ok to keep it reference with those warnnings ?
Those supplies are for a Intel Ethernet controler 10G. This is very important to have good powers supplies.
Thank you in advance for your reply.
Best regards