Post Go back to editing

Extending protection for reverse polarity beyond -40V

Category: Hardware
Product Number: LTC4367

Dear all,

The limit on reverse polarity protection for this device to be -40V is well understood, so an alternative must be found if you're potentially powering from (say) a 48V supply.

Can I ask if a low drop diode in series with the ground connection for the device could be a suitable answer? I'm thinking low-drop Schottky could be used to ensure current flows the correct way through the device. It would apply a small offset to the shutdown and fault pins, but that should be manageable. The OV comparator could also be referenced to the same node. Is the gate guaranteed to be low in this condition?

Something like this:

Any thoughts?

Parents
  • Hi,

    1. Please follow the orientation of the MOSFETs in the application circuit of both LTC4380 (common drain) and LTC4367 (common source). However, in this case, since LTC4380 handles the reverse protection, the LTC4367 can actually be used with a single MOSFET and reverse input protection can still be achieved. 

    As attached in the simulation below.

    In the case of the LTC4380, M2 in the Figure 5of the datasheet has to have a VDS rating >> the expected reverse voltage as its body diode will be the one to block the negative input.
     

    2. If you want to disable current limit in the LTC4380, you can short the SNS pin to the OUT pin. I understand at high load currents, the sense resistor introduces a significant power loss. Please see info from datasheet.
     

       


     

Reply
  • Hi,

    1. Please follow the orientation of the MOSFETs in the application circuit of both LTC4380 (common drain) and LTC4367 (common source). However, in this case, since LTC4380 handles the reverse protection, the LTC4367 can actually be used with a single MOSFET and reverse input protection can still be achieved. 

    As attached in the simulation below.

    In the case of the LTC4380, M2 in the Figure 5of the datasheet has to have a VDS rating >> the expected reverse voltage as its body diode will be the one to block the negative input.
     

    2. If you want to disable current limit in the LTC4380, you can short the SNS pin to the OUT pin. I understand at high load currents, the sense resistor introduces a significant power loss. Please see info from datasheet.
     

       


     

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.