Dear Sir or Madam,
do you have any reommandations or suggestions related to driving the MODE_PLLIN with a modulated carrier. Similar to using spread spectrum.
Does the internal PLL have any limitations on this? Bandwidth?
Best Regards,
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
LTM4662
Recommended for New Designs
The LTM4662 is a complete dual 15A or a single 30A output switching mode DC/DC power supply. Included. Operating from an input voltage range of 4.5V to...
Datasheet
LTM4662 on Analog.com
Dear Sir or Madam,
do you have any reommandations or suggestions related to driving the MODE_PLLIN with a modulated carrier. Similar to using spread spectrum.
Does the internal PLL have any limitations on this? Bandwidth?
Best Regards,
Hello,
In order for the controller to work accordingly the MODE must be within the required frequency:
Required input frequency range (250kHz to 1MHz
Recommended operating range (300kHz to 750kHz
±30% capture range around the programmed frequency for reliable lock
Modulated frequency may not work or can cause a fault in the PLL.
Thanks.