Post Go back to editing

POE+/12VDC

Thread Summary

The user inquired about using the LTC9105 with a 12 VDC auxiliary source for an ESP32-based industrial monitoring gateway, but the LTC9105 is not suitable for voltages below 37V. The support engineer recommended the MAX5996C for 12V auxiliary inputs, which provides telemetry via the MEC pin, and suggested using the MAX5974B/D as a DC-DC converter. The user confirmed this approach aligns with their requirements and requested a specific evaluation/reference schematic for the MAX5996C + 12V auxiliary design.
AI Generated Content
Category: Hardware
Product Number: LTC9105

We initially became interested in the LTC9105 for an ESP32 based industrial monitoring gateway because of its I²C telemetry and PoE power-allocation reporting. However, its datasheet shows a higher-voltage input/AUX architecture that does not appear to directly accommodate a 12 VDC auxiliary source. Is that indeed the case? Alternatively, we reviewed the LTC4278 because its auxiliary input range appears much better suited to a 12 VDC source, although it does not appear to provide the same telemetry capabilities. For our application, we are particularly interested in power telemetry. Ideally, the host processor could determine:

• Whether the active source is PoE+ or external 12 VDC
• Input voltage, current and power consumption
• PoE classification/allocated power, if practical
• Presence/status of the alternate power source

Edit Notes

corrected post
[edited by: Rob1887 at 4:56 PM (GMT -4) on 20 Sep 2026]
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.