Post Go back to editing

Minimum load current requirement for LT1961 application

Category: Datasheet/Specs
Product Number: LT1961

Hello

We have selected LT961 in our design to derive 24V, 20mA output from 15V Input.

From the LTspice simulation, the voltage waveform at SW node is observed as distorted (not turning off) at output current values lower than 120mA. Please see the below image.

However, At Iout > 120mA, the waveform is a perfect square.

Does this IC require a minimum load current to maintain regulation? The datasheet does not explicitly specify a minimum output current requirement.

Update: VSW waveform in blue. Simulation run time = 500ms, I load = 2.5mA [only an LED connected at the output]. 

Edit Notes

Added image of simulation having runtime= 500ms.
[edited by: eenair at 5:27 AM (GMT -4) on 18 Sep 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.