Dear All,
Just asking a hypothetical question here - has anyone ever tried using one of these devices with a relatively constant input voltage, and created a variable output voltage? The potential use case we're considering would require 44-52V input with 30V-100V output at around 50A maximum; maximum power output in the 3kW range.....we would feed the voltage feedback error amplifier with a variable voltage generated by a DAC to control Vout. I have seen MCU to SMPS controller links via I2C, but nothing I have found has the voltage/current capability we would need.
Thanks for any suggestions.