Post Go back to editing

Can I use separate voltages for SVIN (5V) and PVIN (1.8V-2.5V) on the LTC3623??

Category: Datasheet/Specs
Product Number: LTC3623

Hi ADI Support Team,

I am currently working on a power supply design using the LTC3623 and would like to verify if a specific split input voltage configuration is valid.

Based on my system's power rails, I am planning to configure the inputs as follows:

  • SVIN: Fixed 5V

  • PVIN: Variable between 1.8V and 2.5V

The reason for this setup is that my main power input for the converter (PVIN) is variable, ranging from 1.8V to 2.5V.

While I do have a stable 5V rail available in the system, its power capacity is very limited and cannot support the heavy load current required by the main power path (PVIN).

Therefore, I would like to use this 5V rail exclusively to power SVIN to ensure stable operation of the internal circuitry and gate drivers.

Could you please clarify the following?

  1. Is this configuration (SVIN = 5V, PVIN = 1.8V to 2.5V) fully supported and reliable for the LTC3623? Are there any power sequencing requirements between SVIN and PVIN that I should be aware of?

  2. What is the expected maximum bias current required by the SVIN pin under normal switching operation? I need this information to ensure my low-power 5V rail can safely handle the SVIN load.

Any guidance, reference designs, or recommendations would be greatly appreciated.

Thank you in advance!

  • Hi ADI Support Team,

    I just wanted to gently follow up on this thread. Could you let me know roughly when I might expect some feedback on this configuration?

    Please let me know if you need any further details about my system to clarify the question.

    Thank you!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.