Post Go back to editing

LT7809 eval board and our board has startup problems when device is cold

Thread Summary

The user reports unexplained rising output voltage on the LT7809-AZ eval board and a custom board when the chip is below room temperature, with the voltage stabilizing after 20-50 seconds. The issue is resolved when the chip is warmed above 25°C. The problem occurs with both external and internal voltage references, and the output voltage is approximately 26V with an input of 45-50.4V.
AI Generated Content
Category: Hardware
Product Number: LT7809

With both the eval-LT7809-AZ as well as our own board much like the eval board I see unexplained rising output when the chip is below room temp

The voltage will get to target voltage but it can take 20 to 50 seconds.  The voltage ramps up to some value such as 15V then gradual does jumps up (and back down) several volts over many seconds

If I warm the LT7809 mildly to just above 25C room temp everything works well including expected slow start ramp of 20msec.  

I have used the eval board and our own board on-board voltage source for EXTVCC or use chip internal reference, both seem to have same issue.  This is AFTER the choice of voltage to use for bias and may be some internal chip reference.

If I cool down the chip or even have it start up first time in the morning where room temp is 20C or lower I can see unexpected output rise.

This is on the eval board as well as our own board..  In both the eval and our own board this happens.  

The chip has code  B61779 in both cases.

Is this a known issue with next rev chip planning to look at this or is thing new and unknown issue to your team?

Parents
  • Hi Mark,

     

    Please tell me the simplest unmodified Eval Board test conditions/setup to duplicate the issue and which waveforms are wrong. Please send scope captures if possible.

     

    We have engineers trying to replicate the issue now. Is the SS pin resetting on startup?

     

    Best,

    Vanessa Roque

Reply
  • Hi Mark,

     

    Please tell me the simplest unmodified Eval Board test conditions/setup to duplicate the issue and which waveforms are wrong. Please send scope captures if possible.

     

    We have engineers trying to replicate the issue now. Is the SS pin resetting on startup?

     

    Best,

    Vanessa Roque

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.