We are using the LTC4368 in a 24 V protection circuit designed according to the datasheet.
The UV and OV resistor network was calculated using the equations provided in the datasheet with the following resistor values:
- R1 = 3.9 MΩ
- R2 = 243 kΩ
- R3 = 59 kΩ
The intended protection thresholds are:
- Undervoltage (UV): 7 V
- Overvoltage (OV): 36 V
These values were also verified through simulation, which produced the expected operating range of 7 V to 36 V.
But in hardware its coming UV: 2v and OV: 53v