Post Go back to editing

ADM1273 : condition for FET HEALTH FAULT at startup

Category: Datasheet/Specs
Product Number: ADM1273

Hello,

We wanted to test ADM1273 functionality to determine if we can use it for a bidirectional power converter.

I wanted to test the case where the power come from The VOUT side. The IC can start using the mosfet body diode. However, when the VIN voltage exceeds undervoltage threshold and the IC enters start-up mode, it trigger in FET HEALT FAULT. When disenabled this fault before the start-up mode and re-enable it afterward, this fault doesn’t occur. In the Vin to Vout direction, I don’t have this problem. I am unable to determine which condition causes the fault to trigger.

We did our tests with the EVAL-ADM1273 board which I modified to change thresholds. The new thresholds are listed below:

  • overvoltage threshold, OV = 28.3V
  • undervoltage thresholds: UVL = 18.9V, UVH = 21V
  • power good threshold: Vpwrgd =19.2V
  • operating current threshold: ISET = 5.14A

 

Thank u in advance for your help,

  • The ADM1273 is primarily designed as a unidirectional hot-swap controller rather than a bidirectional power-path controller. In the reverse-power scenario where VOUT is energized before VIN, the device can initially power through the MOSFET body diode; however, when VIN rises above the UVH threshold and the ADM1273 enters its startup sequence, the FET Health monitoring may detect this operating condition as a fault and assert a FET Health Fault. The fact that the fault no longer occurs when FET Health monitoring is disabled during startup suggests that the reverse-powered startup condition is outside the device's intended operating mode

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.