Post Go back to editing

Inverting Application

Category: Hardware
Product Number: LT3840

Hi,

Is LT3840 applicable to inverting output voltage? From the LTSpice, I follow the circuit design from the datasheet which I couldn't get the output voltage and current output rating as stated. 

My parameters are:

1. VIN is 24V

2. VOUT can be adjustable from -9V to -17V

3. Output current rating should be at least 20A and above, able to achieve?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.