Post Go back to editing

Extremely low efficiency of the LTC3108

Category: Datasheet/Specs
Product Number: LTC3108

When using an LTC3108 for energy harvesting from a TEG with a 1:100 ratio transformer, the voltage measured at the TEG outputs is 37 mV already connected; the capacitor connected to the Vout pin is 50 mF (with very low losses and low ESR), and pins VS1 and VS2 are configured to obtain 4.1 V at Vout.
The generated current is less than 0.2 µA, meaning the system efficiency is far lower than specified in the datasheet (up to 38%)
Is the problem due to the value of the output capacitor (Cout)? Is it possible? Or where might the problem be coming from?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.