Post Go back to editing

Stabilizing the regulation loop

Thread Summary

The user inquired about selecting the value of Rc for the Vc pin in the LT8376 LED driver when using large output capacitors (Cout > 10uF). Analog Devices tech support advised that there is no detailed mathematical equation for this, recommending placeholders on the board and using LTspice FRA for loop response verification. For analog dimming, stability issues can arise with marginal compensation, unlike PWM dimming. The user found that using real-world component models in LTspice helped identify appropriate values for Rc and Cc, suggesting the datasheet be updated to clarify the typical requirement for Rc.
AI Generated Content
Category: Hardware
Product Number: LT8376

Regarding the selection of the value of Rc connected to the "Vc" pin, the datasheet says the following:

When using an output capacitor Cout larger than 10uF, as is needed for large PWM dimming ratios, a resistor Rc in
series with Cc is also necessary. Larger values of COUT require larger values of RC. See Typical Applications for
some examples.

Looking at the "Typical Applications", it is hard to make out any definitive pattern. 

Cout = 4.7uF uses Rc = 0 & Cc = 0.01uF - LED Driver with Duty Cycle LED Current
Cout = 20uF uses Rc = 20k & Cc = 0.01uF - 24V Voltage Regulator with Spread Spectrum
Cout = 10uF uses Rc = 16k & Cc = 0.0001uF - EMI performance
Cout = 22uF uses Rc = 162k & Cc = 0.01uF - 2A LED Driver with Internal PWM Dimming
Cout = 4.7uF uses Rc = 517k (or 30k) & Cc = 0.00047uF - Multiple String Drivers from Single Boosted 56V Input

Some small values of Vout use very large values for Rc while  others do not.  A 20uF (2 x 10) Vout uses Rc of 20k while a 22uF Vout makes a big jump to 162k.

Isn't there some calculation available to better define what value actually should be used or is this a matter of leaving space on the board for the component and figuring out something that works after it is all assembled?

Does any of this change if analog dimming is being used rather than PWM dimming?  

Parents
  • on Aug 6, 2026 10:16 AM Contains AI Generated Content
    +1

    AD tech support contacted me outside this forum and this was the exchange which took place:

    AD:

    For LED drivers, we dont have a detailed mathematical equation to help calculate the compensation components. 

    I would recommend you have place holder for the components in your board. 

     

    You can also find the application schematics shown in datasheet closest to your application and start with those compensation components. 

    Other option as a starting point is to use LTSPICE FRA tool to verify your design loop response in LTSPICE. 

    We do provide an example on how to setup for LED driver in examples folder. I am attaching that for reference in email here. 

    This example is for a different LED driver, but similar FRA can be performed on LT8376. 

     

    With regards to analog vs PWM dimming, analog dimming LT8376 regulates LED current by changing the current regulation threshold. 

    As a result if compensation is marginal, it could result in stability issues as you change control voltage. 

    For PWM dimming LED current amplitude remains unchanged, converter regulates the same LED current whenever PWM signal is higher. 

    Me:

    I, with the help of Google’s AI, managed to find my own answer to this question along with an answer to a previous unanswered AD tech support question.

    The details are here in this other EngineerZone topic on this component:

      https://ez.analog.com/design-tools-and-calculators/ltspice/f/q-a/602285/ad-supplied-model-oscillates-when-more-realistic-components-used

     It turns out that there are, to some degree, equations which can be used in the solution to this. The LTspice model, which I’m already familiar with (at least the transient response; thanks for the FRA example), can indeed be of some help, but with caveats.  The model that uses ideal components is mostly worthless in this regard because it shows the circuit being stable even if “Rc” is omitted.  The same model, but using real-world representations of components, suffers a bad oscillation if “Rc” is omitted and it can be brought under control if acceptable values of “Rc” and “Cc” are selected/used.  I am indeed using only analog dimming in my application.

     Note that the LT8376 datasheet does its user base a disservice by saying “Stabilizing the regulation loop typically requires only a capacitor Cc connected from the VC pin to GND.”

     An examination of the “Typical Applications” shows only one out of six that have “only” the Cc capacitor so it is definitely NOT “typical”.  Someone at AD needs to reword this datasheet/sentence to something like the following:  “In some cases, where the output capacitance, Cout, is less than 10uF, the Rc resistor may not be required (i.e., 0 ohms) for loop stabilization. Typically however, Rc is required, with larger values of Rc and Cc providing more stable operation and slower response to the control input. The frequency of the compensation loop is given by the following equation  and this needs to be less than the loop crossover frequency for the system (less easily determined).

     

    The AI suggested that the loop crossover frequency is determined in the following manner, though I let it do the calculations and suggest appropriate values for Rc and Cc, which I subsequently tested using the LTspice simulator and more real-world models for the components (see other discussion for that tale).

Reply
  • on Aug 6, 2026 10:16 AM Contains AI Generated Content
    +1

    AD tech support contacted me outside this forum and this was the exchange which took place:

    AD:

    For LED drivers, we dont have a detailed mathematical equation to help calculate the compensation components. 

    I would recommend you have place holder for the components in your board. 

     

    You can also find the application schematics shown in datasheet closest to your application and start with those compensation components. 

    Other option as a starting point is to use LTSPICE FRA tool to verify your design loop response in LTSPICE. 

    We do provide an example on how to setup for LED driver in examples folder. I am attaching that for reference in email here. 

    This example is for a different LED driver, but similar FRA can be performed on LT8376. 

     

    With regards to analog vs PWM dimming, analog dimming LT8376 regulates LED current by changing the current regulation threshold. 

    As a result if compensation is marginal, it could result in stability issues as you change control voltage. 

    For PWM dimming LED current amplitude remains unchanged, converter regulates the same LED current whenever PWM signal is higher. 

    Me:

    I, with the help of Google’s AI, managed to find my own answer to this question along with an answer to a previous unanswered AD tech support question.

    The details are here in this other EngineerZone topic on this component:

      https://ez.analog.com/design-tools-and-calculators/ltspice/f/q-a/602285/ad-supplied-model-oscillates-when-more-realistic-components-used

     It turns out that there are, to some degree, equations which can be used in the solution to this. The LTspice model, which I’m already familiar with (at least the transient response; thanks for the FRA example), can indeed be of some help, but with caveats.  The model that uses ideal components is mostly worthless in this regard because it shows the circuit being stable even if “Rc” is omitted.  The same model, but using real-world representations of components, suffers a bad oscillation if “Rc” is omitted and it can be brought under control if acceptable values of “Rc” and “Cc” are selected/used.  I am indeed using only analog dimming in my application.

     Note that the LT8376 datasheet does its user base a disservice by saying “Stabilizing the regulation loop typically requires only a capacitor Cc connected from the VC pin to GND.”

     An examination of the “Typical Applications” shows only one out of six that have “only” the Cc capacitor so it is definitely NOT “typical”.  Someone at AD needs to reword this datasheet/sentence to something like the following:  “In some cases, where the output capacitance, Cout, is less than 10uF, the Rc resistor may not be required (i.e., 0 ohms) for loop stabilization. Typically however, Rc is required, with larger values of Rc and Cc providing more stable operation and slower response to the control input. The frequency of the compensation loop is given by the following equation  and this needs to be less than the loop crossover frequency for the system (less easily determined).

     

    The AI suggested that the loop crossover frequency is determined in the following manner, though I let it do the calculations and suggest appropriate values for Rc and Cc, which I subsequently tested using the LTspice simulator and more real-world models for the components (see other discussion for that tale).

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.