Post Go back to editing

Temperature setpoint with DAC

Thread Summary

The user is trying to adjust the temperature set point and range of a Peltier controlled by an ADN8835 TEC controller from 15-35°C to 10-60°C. The current setup uses a 1.25V reference at IN1N and a 10k+10k voltage divider at IN2P. The final answer indicates that a TEC applications engineer will review the request. The AD5593RBCPZ DAC can generate 0-2.5V to override the set point.
AI Generated Content
Category: Hardware
Product Number: ADN8835

We having a board which uses the ADN8835 TEC controller to control the temperature of a Peltier. The temperature set point is set to 25 degrees with a span of 10 degrees up and down using the circuit below.

If I understand it correctly, this is because IN1N is 1.25V at 25 degrees Celcius an IN2P is always 1.25V because o the 10k+10k voltage divider. We can overrule this set point, by driving a different voltage on the IN2P pin. This is connected to a DAC (AD5593RBCPZ) which can generate a voltage from 0 to 2.5V (TEC_PIC1_VREF voltage in the schematic below).

Now our customer would like to have a different temperature set point and much wider range (for example 10-60 degrees). I can't figure this out with the datasheet.

Would it be possible to change the set point and range? If so, how can this be calculated?

Thanks in advance!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.