I had a MAX17521 project saved in EESim, which did not transition to the new Power Studio Designer and I cannot find this device in the new tool. This is a problem! Is there still a way to access the old EESim tool?
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 1 hours |
Awaiting Company Response | |
MAX17521
Production
The MAX17521 dual-output, high-efficiency, high-voltage, synchronous step-down DC-DC converter with integrated MOSFETs operates over a 4.5V to 60V input...
Datasheet
MAX17521 on Analog.com
I had a MAX17521 project saved in EESim, which did not transition to the new Power Studio Designer and I cannot find this device in the new tool. This is a problem! Is there still a way to access the old EESim tool?
I am looking into this. I also saw your other case on this.
John
Thanks! This really came at a bad time...
(and yeah I had some issues with some profile settings and may have inadvertently submitted a duplicate/redundant case)
Status update please?
The Release on July 30 th should have the MAX17521 in it.