Post Go back to editing

Inductor DCR current sensing for LT8292 (instead of discrete shunt resistor)

Thread Summary

The user inquired if the LT8292 can use inductor DCR current sensing like the LTC7891. The final answer confirms that the LT8292 does not support DCR sensing due to high LSN pin leakage current, which introduces significant error. A direct current sense resistor is recommended for the LT8292.
AI Generated Content
Category: Hardware
Product Number: LT8292

Hello,

I am using an LT8292 and also a LTC7891 in a design.  The LTC7891 explicitly calls out inductor DCR current sensing as a technique to avoid use of a discrete shunt, as well as a detailed procedure for choosing the corresponding passive components.  The LT8292 doesn't mention that technique in its datasheet.  Can I use the same technique for the LT8292, or is this not recommended for a specific reason?  The inductor DCR (3.8-4.3mOhm) is much larger than the resistance of any shunt I would want to use (~1mOhm) so this would provide a larger signal for the current control.  Obviously the inductor DCR is less precise, but I don't have a sense of how to trade-off these attributes.

Thanks!

Sam

Parents
  • Hi,

     

    I just heard back from the designer. They confirmed that the LT8292 does not support DCR current sensing. The LSN pin leakage current is too high for a DCR sensing network and introduces a large error voltage that can dominate the sensed signal, preventing proper current sensing operation.

    A direct current sense resistor should be used with LT8292 as shown in the datasheet. DCR sensing is not a supported or recommended configuration for this family.

    Thanks!

Reply
  • Hi,

     

    I just heard back from the designer. They confirmed that the LT8292 does not support DCR current sensing. The LSN pin leakage current is too high for a DCR sensing network and introduces a large error voltage that can dominate the sensed signal, preventing proper current sensing operation.

    A direct current sense resistor should be used with LT8292 as shown in the datasheet. DCR sensing is not a supported or recommended configuration for this family.

    Thanks!

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.