Hi,
For MAX25252, can I tie the outputs after the power inductors of OUT2 and OUT3 rails together? If so, how should I connect the Sense Inputs (pins 7&13)? Tie these 2 pins together, too?
Thank you,
Tony
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 64 hours |
Closed | |
MAX25252
Recommended for New Designs
The MAX25252 is a high-efficiency, five-output ASIL B PMIC with three DC-DC converters, and two high-PSRR LDOs, with OV/UV monitoring on all outputs. OUT1...
Datasheet
MAX25252 on Analog.com
Hi,
For MAX25252, can I tie the outputs after the power inductors of OUT2 and OUT3 rails together? If so, how should I connect the Sense Inputs (pins 7&13)? Tie these 2 pins together, too?
Thank you,
Tony
BTW, may I get the user manual of the MAX25252EVKIT board?
Hi
This part is a NDA device on the NDA parts you will need to go to the person that gave you the datasheet and other information and ask them for support.
These parts are not supported through Engineer Zone or the email and portal system.
Tony, let me connect you with the factory apps expert on MAX25252 and we'll try to answer your questions. Best regards.
Hello @TonyC,
Warren brought this to my attention. How did you come to learn about MAX25252 and the EVKIT?
Thanks!
Hi PTran,
We have a special need for 4.1V and 3.6V power rails and this PMIC meets our requirements. We'd like to order an eval board to test this chip.
Thank you,
Tony
Hello TonyCelero ,
Please have your ADI contact place an order for the MAX25252 EVKit. The EVKit is introduced.
MAX25252EVKIT Evaluation Board | Analog Devices
Thanks,
Phillip
Hi Philip,
I actually don't have an ADI contact. My purchasing will try to buy it online. If he can't, I'll let you know. I did go to the eval board page but it doesn't show the design details. Do you have a user manual that you can share?
Thank you,
Tony