Post Go back to editing

Reliability issues

Thread Summary

The user experienced issues with the LTC7000 MOSFET driver not fully enhancing the MOSFETs, resulting in only half the intended gate voltage. The final answer suggests adding a diode to the TS pin and considering current-sharing ballasting or using a larger single FET. The accompanying answer shows a scope trace indicating improved performance with a diode, suggesting a flyback diode is necessary for better undershoot protection.
AI Generated Content
Category: Hardware
Product Number: LTC7000A

I have been experiencing issues with the LTC7000 mosfet driver. It is used as a static switch driver in a failsafe system for depowering an electronic speed controller. What happens is that over some extended use the driver will no longer fully enhance the MOSFET, only getting about half the intended gate voltage. The connected ESC is driving a moderately sized motor load at 11-13A and about 8V. So far i am suspecting that it might be because we lack a diode at the TS pin, but please do tell me if there are other obvious issues.

Attached are pictures of the schematic we used, as well as the PCB design:

/resized-image/__size/640x480/__key/communityserver-discussions-components-files/330/pastedimage1783422417790v2.png

/resized-image/__size/640x480/__key/communityserver-discussions-components-files/330/pastedimage1783422605608v3.png

/resized-image/__size/640x480/__key/communityserver-discussions-components-files/330/pastedimage1783422656809v4.png

Parents
  • Here is a scope trace of the TS pin with and without a diode. This is the moment a large motor is switched off by the static switch. it seems that the undershoot is better with a diode, but it could be better with a purpose selected diode(the one i used was just a random one we had laying around). So the lack of a flyback diode was the most likely cause.

Reply
  • Here is a scope trace of the TS pin with and without a diode. This is the moment a large motor is switched off by the static switch. it seems that the undershoot is better with a diode, but it could be better with a purpose selected diode(the one i used was just a random one we had laying around). So the lack of a flyback diode was the most likely cause.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.