Post Go back to editing

LT8722 Maximum Supply Voltage for reliable operation

Thread Summary

The user inquires about increasing the supply voltage for the LT8722 from 12 V to 14 V or 15 V. The final answer confirms that the LT8722's VIN limit is 15 V, both for recommended and absolute maximum operation. It is advised to stay closer to 14 V to ensure the worst-case peak voltage remains under 15 V, avoiding any risk to the IC's lifetime.
AI Generated Content
Category: Hardware
Product Number: LT8722

Hello,

we are currently using the LT8722 in an existing product and want to switch to a different peltier element with a higher nominal voltage. Currently we are supplying it with 12 V generated by another buck converter with about 100 mV ripple under full load. Can we increase it to 14 V or even 15 V without significantly compromising the lifetime of the IC?

Kind regards

Edit Notes

Adjust title
[edited by: mkeller at 10:13 PM (GMT -4) on 10 Jul 2026]
  • The LT8722 is only guaranteed to operate within the conditions specified in the datasheet. 

    For VIN the limit is 15 V. Importantly that's both the recommended operating max and the absolute maximum. There's no margin band above it.

     

    There is no lifetime concern for the part as long as you stay within the specified operating conditions. So I'd recommend staying closer to 14 V (or lower) to give enough headroom that your worst case peak stays under 15V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.