Post Go back to editing

1 A Voltage Controlled Voltage Source using LT3080 and DAC output anomaly

Thread Summary

The user is experiencing issues with the LT30800EQ LDO where the output voltage does not return to 0 V when the DAC is set to 0 V, but operates normally for higher voltages. The final answer suggests reviewing the basic concept of controlling an LDO output with a DAC and provides a link to a detailed discussion on the LT3090 for further guidance. The intermittent behavior when the DAC is set to a voltage above 3.3–4.2 V before returning to 0 V is noted.
AI Generated Content
Category: Hardware
Product Number: LT3080

Dear Analog Devices Technical Support Team,

I am designing a voltage-controlled voltage source using the LT30800EQ, where the output voltage is controlled by a DAC connected to the SET pin.

However, I am observing an unexpected behavior when commanding the DAC to output low voltages. In some cases, when the DAC is set to 0 V, the output does not return to 0 V as expected and instead remains at approximately 3.3–4.2 V. Interestingly, the DAC appears to operate normally when commanded to output voltages above this range.

I have also noticed that, on occasion, the DAC can successfully return to 0 V after first being set to a voltage above the 3.3–4.2 V range. This behavior is intermittent and difficult to reproduce consistently.

Could you please advise whether there are any considerations, limitations, or design issues related to driving the LT3080 SET pin directly from a DAC that might explain this behavior? Have I overlooked anything in the implementation?

I have attached the schematic for reference.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.