Post Go back to editing

Adding Shutdown when LT3083 in parallel

Category: Datasheet/Specs
Product Number: LT3083

In LT3083 datasheet, an example was given to add Shutdown when a single LT3083 is in used.    Another example was given showing how to use LT3083 in parallel.

How to add Shutdown when two LT3083 are used in parallel?

At the SET pin, it seems follow the example when single LT3083 is used.

However, at OUT, do I need 2 Q2 to connect to OUTs or 1 Q2 to connect to VOUT (after ballast resistors) ?

Thanks in advanced.

Anwar

Edit Notes

Correction
[edited by: TheOptim at 8:00 AM (GMT -4) on 22 Jun 2026]
Parents
  • Hi Harshal,

    Thank you for the reply.  From LTspice simulations, using one Q2 transistor after ballast resistors, I can't get true zero Vout when in shutdown, especially for low loads.

    In my application, since LT3083 VControl is separate from VIN, I decided to use reed relay to disconnect supply to VControl when shutdown is required.  Using this method, Vout is truly zero in shutdown.

    Regards,

    Anwar

Reply
  • Hi Harshal,

    Thank you for the reply.  From LTspice simulations, using one Q2 transistor after ballast resistors, I can't get true zero Vout when in shutdown, especially for low loads.

    In my application, since LT3083 VControl is separate from VIN, I decided to use reed relay to disconnect supply to VControl when shutdown is required.  Using this method, Vout is truly zero in shutdown.

    Regards,

    Anwar

Children
No Data