Post Go back to editing

LTM8045 Model FB Pin Regulation Incorrect

Category: Datasheet/Specs
Product Number: LTM8045

Below is my circuit, I am attempting to convert +5V into a -11.5V output:


The FB resistor is calculated using the formula in the datasheet to be 138.1Kohms.


Why is FB regulating to -8mV? Is my circuit incorrect or is this a model issue? Are there considerations with my circuit design that I missed? Vout is around -11.6V, not the -11.5V that was set.

Edit Notes

Added output voltage clarification.
[edited by: Yibo at 7:00 PM (GMT -4) on 18 Jun 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.