LTM4637
Recommended for New Designs
The LTM4637 is a complete 20A output high efficiency switch mode step-down DC/DC μModule (power module) regulator. Included in the package are the switching...
Datasheet
LTM4637 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Hello Team,
I have a question regarding the LTM4637 µModule regulator.
I am trying to generate a 5.5 V output from a 12 V input supply. Based on the datasheet, the device supports 5.5 V output with load currents in the range of approximately 10–15 A.
I performed a simulation in LTspice, and while I am able to obtain an output close to 5.5 V, I am seeing some variation, and the output is not stable or exactly at the expected value.
For the feedback network:
I would like to understand:
I have attached my schematic for reference. Kindly review it and let me know if there are any mistakes or improvements needed.
Thanks,
Surya

Hi SGCH ,
Can you upload your LTspice schematic, symbol and model files? Zip up and drag to this window.
mike
LTspice Team
Hi MStokowski,

Thanks,
Surya
Hi SGCH ,
It's best if you upload your schematic files. Drag to the window, or Choose Insert > Image/Video/File and then click upload in window that appears.
mike
Hi Team,
Please find the attached simulation files for your reference. Kindly review and provide your feedback.
LTM4637.ascLTM4637.rawLTM4637.op.raw
LTspice 24.1.8 for Windows Circuit: C:\Users\suryaganesh.c\Documents\LTspice\LTM4637.net Start Time: Thu Jun 4 14:36:42 2026 solver = Normal Maximum thread count: 8 tnom = 27 temp = 27 method = trap Direct Newton iteration failed to find .op point. (Use ".option noopiter" to skip.) Starting Gmin stepping Gmin = 10 Gmin = 1.07374 Gmin = 0.115292 Gmin = 0.0123794 Gmin = 0.00132923 Gmin = 0.000142725 Gmin = 1.5325e-05 Gmin = 1.6455e-06 Gmin = 1.76685e-07 Gmin = 1.89714e-08 Gmin = 2.03704e-09 Gmin = 2.18725e-10 Gmin = 2.34854e-11 Gmin = 2.52173e-12 Gmin = 2.70769e-13 Gmin = 0 Gmin stepping succeeded in finding the operating point. Total elapsed time: 4.864 seconds. Files loaded: C:\Users\suryaganesh.c\Documents\LTspice\LTM4637.net C:\Users\suryaganesh.c\AppData\Local\LTspice\lib\sub\LTM4637.sub
Thanks,
Surya