Post Go back to editing

Can I use the LT3092 with negative voltages?

Thread Summary

The user inquired about using the LT3092 as a current limiter with a negative voltage regulator (LT337) to limit current while maintaining a stable negative voltage. The support engineer confirmed that the LT3092 can operate in a negative voltage environment, but the voltage across the load will vary with the load current, making it unsuitable for the user's application. The user then proposed using a variable load like a photodiode, but the engineer noted that the LT3092 would still limit current, affecting the load voltage, and thus not meeting the requirement for stable voltage regulation.
AI Generated Content
Category: Hardware
Product Number: LT3092

I have a question regarding the operation of the LT3092. To demo its functionality as a programmable current source, I was able to simulate it in LTspice with the LT317A Positive Voltage Regulator to give the regulator a current limiting functionality. However, I was wondering if it could also work for negative voltages as well? For example, in the example image below, I would have the LT3092 in series with the LT337 negative voltage regulator to limit the current from the voltage regulator. Would this be okay as long as the voltages are within spec of the part (i.e., below 40 volts)?

Parents Reply Children
No Data