Post Go back to editing

LT8210 - Compensation network calculation for RC1, CC1 and CP1

Category: Datasheet/Specs
Product Number: LT8210

Hi ADI engineers,

I am designing a 24 V buck-boost converter using the LT8210. The input voltage range is 18 V to 57 V, and the required output current is 12 A.

I am currently working on the stability compensation and trying to determine the correct values for RC1, CC1, and CP1. I would appreciate guidance on the following:

  • How should I calculate RC1, CC1, and CP1 for this operating range?

  • Are there recommended equations or design procedures for the LT8210 compensation network?

  • Are there any stability considerations specific to a wide input range and 12 A load?

If helpful, I can also share my schematic, switching frequency, inductor value, and output capacitor selection.

Thank you.

Jolly Jacob

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.