Post Go back to editing

LTC4418 - using INTVCC to power external low-power circuitry

Thread Summary

The user asked if it is permissible to draw a small amount of external load current from the INTVCC pin of the LTC4418 to power low-power external components. The final answer from Analog Devices states that it is not recommended to draw current from INTVCC, as it is intended for internal use by the IC.

View FAQ
AI Generated Content
Category: Hardware
Product Number: LTC4418

Hello, I'm designing a power priority switch using the LTC4418 and I have a question regarding the INTVCC pin.

In the typical application circuit, INTVCC is only shown with a 100 nF bypass capacitor to GND, and the datasheet describes it as the internal 3V3 regulator output used by the IC itself.

My question: Is it permissible to draw a small amount of external load current from INTVCC to supply low-power external components, such as:

  • A small logic gate or buffer
  • Pull-ups for logic signals
  • A low-power microcontroller in sleep / idle mode
  • etc

If yes, what is the maximum recommended external load current on INTVCC without affecting LTC4418 operation?

Thank you in advance for any guidance.

Best regards,

Milan