Post Go back to editing

LTC4267 isolated 5V will not start

Thread Summary

The user's board with the LTC4267 isolated 5V supply is not starting, likely due to incorrect capacitor configuration. The final answer suggests confirming that C5 or its equivalent is removed or connected between VPORTP and PGND, and recommends sharing a waveform of the detection attempt and specifying the PSE/Injector type. It also notes that for power needs exceeding 13W, newer options are available without the battery circuit in Design Note 361.
AI Generated Content
Category: Hardware
Product Number: LTC4267

I've incorporated the LTC4267 isolated 5V supply as detalied in Design Note 361 (attached). The board will not start; I can see the initial voltage between VPORTP and VPORTN is sufficient to start the internal Rclass detection but that's all; it just repeats the initial ramp. Has anyone used this design and can anyone suggest what might be the problem?PDF

Parents
  • A final twist - the snubber resistor R7 on DN461 is an order of magnitude out; it should be 1K, and best stability without excessive power dissipation is achieved with C3 in the range 330-470pF for the PA1134 transformer specified. With R3 set to 100R, there's unresolveable overshoot on Q1 drain.

Reply
  • A final twist - the snubber resistor R7 on DN461 is an order of magnitude out; it should be 1K, and best stability without excessive power dissipation is achieved with C3 in the range 330-470pF for the PA1134 transformer specified. With R3 set to 100R, there's unresolveable overshoot on Q1 drain.

Children
No Data